AXIS#.MOTOR.TEMPFAULT

Description

This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensorClosed A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.

A zero value prevents temperature faults from being reported.

Context

For more information see Motor and Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Ω

Range

0 to 2,000,000,000 Ω

Default Value

2000

Data Type

Integer

See Also

AXIS#.MOTOR.TEMP

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.MOTOR.TEMPFAULT

500bh

1dh

Unsigned32

-

-

Read/Write

No

AXIS2.MOTOR.TEMPFAULT

510bh

1dh

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TEMPFAULT

6218

184A

Unsigned32

Read Only

-

AXIS2.MOTOR.TEMPFAULT

71754

1184

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TEMPFAULT

6218

Unsigned32

Read Only

-